PSOC® Exp Brd Kit Quick Start Guide Datasheet by Cypress Semiconductor Corp

View All Related Products | Download PDF Datasheet
PSOC® PRECISION ANALOG TEMPERATURE SENSOR EXPANSION BOARD KIT
QUICK START GUIDE
CY8CKIT-025 PSoC Precision Analog Temperature Sensor Expansion Board Kit Contents
Install Software
1. Insert the kit DVD and install the kit software.
2. Refer to the CY8CKIT-025 Kit Guide in
<Install_Directory>\PSoC Precision Analog
EBK\<version>\Documentation for detailed
installation instructions.
3. The projects will be installed at
<Install_Directory>\PSoC Precision Analog
EBK\<version>\Firmware.
Board Setup
1. Verify that jumper J6 is installed for RTD
measurement.
2. Verify that jumper J5 is installed between pins
2 and 3 to use the thermistor on board.
CY8CKIT-012
Prototype Boards
Kit DVD
Omega Thermocouple
K-type
Wires
2N3904 NPN
Transistors
Prototype Headers for
CY8CKIT-012 Board
Quick Start
Guide
Screwdriver
2x20 Pin
Connector for
Development Kit
Interface
r
RTD Section
r
Thermistor Section
r
Diode
Section
r
Thermocouple Section
CY8CKIT-025 Board
1
2
© 2011-2014 Cypress Semiconductor Corporation. All rights reserved. All trademarks or registered
trademarks referenced herein are the properties of their respective owners. Doc #: 001-65531 Rev. *F
http://www.cypress.com/go/CY8CKIT-025
For the latest information about this kit, visit
PSOC® PRECISION ANALOG TEMPERATURE SENSOR EXPANSION BOARD KIT
QUICK START GUIDE
Board Setup
1. Connect the thermocouple at connector J2.
2. Connect 2N3904 transistors at connector J4 for
diode measurement.
Connect with PSoC 3/PSoC 5 Development Kit
1. Connect the CY8CKIT-025 Expansion Board Kit to
Port E of the CY8CKIT-030 PSoC 3 Development
Kit/CY8CKIT-050 PSOC 5LP Development Kit.
2. Power the CY8CKIT-030/CY8CKIT-050 by
connecting the USB cable at J1.
Program the PSoC Device
1. Open TempSense_030_050.cywrk from PSoC
Creator Start Page > Examples and Kits > Kits >
PSoC Precision Analog EBK.
2. Select the location for the example project.
3. Click the Program icon in PSoC Creator.
4. Press the Reset button on the board to restart the kit.
Test the Expansion Board Kit
1. LCD shows the temperature reading.
2. Use the P5_5 and P5_6 CapSense buttons on
CY8CKIT-030/CY8CKIT-050 to select
temperature display of different sensors.
3. Refer to the CY8CKIT-025 Kit Guide, mentioned in
step 1, for information on kit operation and
additional example projects using CY8CKIT-001
and CY8CKIT-030/CY8CKIT-050.
3
4
5
6

Products related to this Datasheet

BOARD PSOC ANALOG TEMP SENSOR