Character
Agglication
Technical Data
Mam
g
[H3
Basic fl 1002
Email: sa‘es@hwsensor,com
Henan Hanwei Electronics Co., Ltd www.hwsensor.com
Tel: 86-371-67169070/80 Fax: 86-371-67169090 Email: sales@hwsensor.com
MQ131 Semiconductor Sensor for Ozone
Sensitive material of MQ131 gas sensor is SnO2, which with lower conductivity in clean air. When
Ozone gas exists. The sensor’s conductivity is more higher along with the gas concentration rising.
Please use simple electrocircuit, Convert change of conductivity to correspond output signal of gas
concentration.
MQ131 gas sensor has high sensitity to Ozone, also sensitive to CL2, NO2, etc.
Character Configuration
* Good sensitivity to Ozone in wide range
* High sensitivity to Ozone
* Long life and low cost
* Simple drive circuit
Application
* Domestic Ozone concentration overload Detector
* Industrial Ozone concentration overload Detector
* Portable Ozone concentration overload Detector
Technical Data Basic test loop
The above is basic test circuit of the sensor.
The sensor need to be put 2 voltage,
heater voltage(VH) and test voltage(VC).
VH used to supply certified working
temperature to the sensor, while VC used
to detect voltage (VRL) on load resistance
(RL)whom is in series with sensor. The
sensor has light polarity, Vc need DC
power. VC and VH could use same power
circuit with precondition to assure
performance of sensor. In order to make
the sensor with better performance,
suitable RL value is needed:
Power of Sensitivity body(Ps): Ps=Vc2×Rs/(Rs+RL)2
Resistance of sensor(Rs): Rs=(Vc/VRL-1)×RL
Model No. MQ131
Sensor Type Semiconductor
Standard Encapsulation Bakelite (Black Bakelite)
Detection Gas Ozone
Concentration 10-1000ppm Ozone
Loop Voltage Vc ≤24V DC
Heater Voltage VH 5.0V±0.2V AC or DC
Circuit
Load
Resistance
RL Adjustable
Heater
Resistance
RH 31Ω±3Ω(Room Tem.)
Heater
consumption
PH ≤900mW
Sensing
Resistance Rs 50KΩ-500KΩ(in 50ppm O3)
Sensitivity S Rs(in air)/Rs(in 50ppm O3)≥3
Character
Slope α (R50ppm/R10ppm O3)
Tem. Humidity 20℃±2℃;65%±5%RH
Standard test circuit Vc:5.0V±0.1V;
V
H: 5.0V±0.1V
Condition
Preheat time Over 48 hours
Vc
VH
GND
RL
VRL
23mm
—-—.—,—o—
_ a H
7
E
a
25m 9 H
r 3
10) I 5
1 1
m ‘ —.— ml ‘ 5
. 4— l 1 \\
é K +0. 3
B \
g \ ~— 03 AA l 1
l W
o 5
o 1
o. 1 - o s
1030 -m 10
Structure and configuration
5 Fans Manuals
1 Gas senswng level SnOZ
Emma: Au
4 4 H Beam-is Ina n
E mam cam mm alloy
3 3 mama. ceramic Alma
Amvraxpluum nemwk sums: 5129‘ gauze
(susm a 1 Elm-mesh)
damp nng Cwnev gleam Nx
Rss‘n bass Bekalne
Tub: Pln Conway ufllng NI
Email: sales@hwsensor.com
Henan Hanwei Electronics Co., Ltd www.hwsensor.com
Tel: 86-371-67169070/80 Fax: 86-371-67169090 Email: sales@hwsensor.com
Sensitivity Characteristics Influence of Temperature/Humidity
Fig.1 shows the typical sensitivity characteristics of Fig.2 shows the typical temperature and humidity
the MQ131, ordinate means resistance ratio of the sensor characteristics. Ordinate means resistance ratio
(Rs/Ro), abscissa is concentration of gases. Rs means of the sensor (Rs/Ro), Rs means resistance of sensor
resistance in different gases, Ro means resistance of in 50ppm Ozone under different tem. and humidity.
sensor in 50ppm CL2. All test are under standard Ro means resistance of the sensor in environment of
test conditions. 50ppm Ozone, 20℃/65%RH
Structure and configuration
Structure and configuration of MQ131 gas sensor is shown as Fig. 3, sensor composed by micro AL2O3 ceramic tube, Tin
Dioxide (SnO2) sensitive layer, measuring electrode and heater are fixed into a crust made by plastic and stainless steel
net. The heater provides necessary work conditions for work of sensitive components. The enveloped MQ-4 have 6 pin, 4
of them are used to fetch signals, and other 2 are used for providing heating current.
\/
/\
u.
Email: sa‘es@hwsensor,com
Henan Hanwei Electronics Co., Ltd www.hwsensor.com
Tel: 86-371-67169070/80 Fax: 86-371-67169090 Email: sales@hwsensor.com
Notification
1 Following conditions must be prohibited
1.1 Exposed to organic silicon steam
Organic silicon steam cause sensors invalid, sensors must be avoid exposing to silicon bond,
fixature, silicon latex, putty or plastic contain silicon environment
1.2 High Corrosive gas
If the sensors exposed to high concentration corrosive gas (such as H2Sz, SOX, Cl2, HCl etc), it will
not only result in corrosion of sensors structure, also it cause sincere sensitivity attenuation.
1.3 Alkali, Alkali metals salt, halogen pollution
The sensors performance will be changed badly if sensors be sprayed polluted by alkali metals salt
especially brine, or be exposed to halogen such as fluorin.
1.4 Touch water
Sensitivity of the sensors will be reduced when spattered or dipped in water.
1.5 Freezing
Do avoid icing on sensor’surface, otherwise sensor would lose sensitivity.
1.6 Applied voltage higher
Applied voltage on sensor should not be higher than stipulated value, otherwise it cause down-line or
heater damaged, and bring on sensors’ sensitivity characteristic changed badly.
1.7 Voltage on wrong pins
For 6 pins sensor, if apply voltage on 1、3 pins or 4、6 pins, it
will make lead broken, and without signal when apply on 2、4 pins
2 Following conditions must be avoided
2.1 Water Condensation
Indoor conditions, slight water condensation will effect sensors performance lightly. However, if water
condensation on sensors surface and keep a certain period, sensor’ sensitivity will be decreased.
2.2 Used in high gas concentration
No matter the sensor is electrified or not, if long time placed in high gas concentration, if will affect
sensors characteristic.
2.3 Long time storage
The sensors resistance produce reversible drift if it’s stored for long time without electrify, this drift is
related with storage conditions. Sensors should be stored in airproof without silicon gel bag with clean air.
For the sensors with long time storage but no electrify, they need long aging time for stbility before using.
2.4 Long time exposed to adverse environment
No matter the sensors electrified or not, if exposed to adverse environment for long time, such as
high humidity, high temperature, or high pollution etc, it will effect the sensors performance badly.
2.5 Vibration
Continual vibration will result in sensors down-lead response then repture. In transportation or
assembling line, pneumatic screwdriver/ultrasonic welding machine can lead this vibration.
2.6 Concussion
If sensors meet strong concussion, it may lead its lead wire disconnected.
2.7 Usage
For sensor, handmade welding is optimal way. If use wave crest welding should meet the following
conditions:
2.7.1 Soldering flux: Rosin soldering flux contains least chlorine
2.7.2 Speed: 1-2 Meter/ Minute
2.7.3 Warm-up temperature: 100±20℃
2.7.4 Welding temperature: 250±10℃
2.7.5 1 time pass wave crest welding machine
If disobey the above using terms, sensors sensitivity will be reduced.
Products related to this Datasheet
OZONE 2 CLICK