STM32MP157(A,C)-EV1 Data Brief Datasheet

KyIW,
STM32MP157C-EV1 top view. Picture
is not contractual.
Features
STM32MP157 Arm®-based dual Cortex®-A7 32 bits + Cortex®-M4 32 bits MPU
in LFBGA448 package
ST PMIC STPMIC1
2 × 4-Gbit DDR3L, 16 bits, 533 MHz
2 × 512-Mbit Quad-SPI Flash
32-Gbit eMMC v5.0
8-Gbit SLC NAND, 8 bits, 8-bit ECC, 4-KB PS
1-Gbit/s Ethernet (RGMII) compliant with IEEE-802.3ab
USB Host 4-port hub
USB OTG HS
CAN FD
5.5" TFT 720×1280 pixels with LED backlight, MIPI DSISM interface, and
capacitive touch panel
SAI audio codec
5-megapixel, 8-bit camera
4 × ST-MEMS digital microphones
• Smartcard
• microSD card
2 user LEDs
2 user and reset push-buttons, 1 wake-up button
4-direction joystick with selection button
5 V / 4 A power supply
Board connectors:
Ethernet RJ45
4 × USB Host Type-A
USB OTG Micro-AB
SPDIF RCA input and output
CAN FD
Stereo headset jack including analog microphone input
Audio jack for external speakers
Motor control
External I2C
– LTDC
Trace, JTAG, RS-232
GPIO expansion connector (Raspberry Pi® shields capability)
MEMS-microphone daughterboard expansion connector
On-board ST-LINK/V2-1 debugger/programmer with USB re-enumeration
capability: Virtual COM port and debug port
STM32CubeMP1 and full mainline open-source Linux® STM32 MPU
OpenSTLinux Distribution (such as STM32MP1Starter) software and examples
Support of a wide choice of Integrated Development Environments (IDEs)
including IAR, Keil®, GCC-based IDEs
Product status link
STM32MP157A-EV1
STM32MP157C-EV1
Evaluation boards with STM32MP157 MPUs
STM32MP157A-EV1 STM32MP157C-EV1
Data brief
DB3800 - Rev 2 - August 2019
For further information contact your local STMicroelectronics sales office.
www.st.com
Description
The STM32MP157A-EV1 and STM32MP157C-EV1 Evaluation boards are the full-
feature demonstration and development platforms for STMicroelectronics Arm®-
based dual Cortex®-A7 32 bits and Cortex®-M4 32 bits MPUs in the STM32MP1
Series. They leverage the capabilities of STM32MP1 Series microprocessors to allow
users develop applications using STM32 MPU OpenSTLinux Distribution software for
the main processor and STM32CubeMP1 software for the co-processor.
They include an ST-LINK embedded debug tool, LEDs, push-buttons, one joystick, 1-
Gbps Ethernet, CAN FD, one USB OTG Micro-AB connector, four USB Host Type-A
connectors, LCD display with touch panel, camera, stereo headset jack with analog
microphone input, four digital microphones, one SPDIF Rx/Tx, smartcard, microSD
card, and eMMC, NOR and NAND Flash memories.
To expand the functionality of the STM32MP157A-EV1 and STM32MP157C-EV1
Evaluation boards, two GPIO expansion connectors are also available for motor
control and Raspberry Pi® shields.
STM32MP157A-EV1 STM32MP157C-EV1
DB3800 - Rev 2 page 2/7
1Ordering information
To order an STM32MP157 Evaluation board, refer to Table 1. For a detailed description of each board, refer to its
user manual on the product web page. Additional information is available from the datasheet and reference
manual of the target STM32.
Table 1. List of available products
Order code Board reference User
manual Target STM32 Differentiating
feature
STM32MP157A-EV1 MB1262: mother board
MB1263: MPU subsystem
daughterboard
MB1230: DSI display board
MB1379: camera board
UM2535
STM32MP157AAA3 Basic security.
STM32MP157C-EV1 STM32MP157CAA3 Secure Boot and
cryptography.
1.1 Product marking
Evaluation tools marked as “ES” or “E” are not yet qualified and therefore not ready to be used as reference
design or in production. Any consequences deriving from such usage will not be at ST charge. In no event, ST will
be liable for any customer usage of these engineering sample tools as reference design or in production.
“E” or “ES” marking examples of location:
On the targeted STM32 that is soldered on the board (for illustration of STM32 marking, refer to the STM32
datasheet “Package information” paragraph at the www.st.com website).
Next to the evaluation tool ordering part number that is stuck or silk-screen printed on the board.
1.2 Codification
The meaning of the codification is explained in Table 2.
Table 2. Codification explanation
STM32MP1XXY-EVZ Description Example: STM32MP157C-EV1
STM32MP1 MPU series in STM32 Arm Cortex MPUs STM32MP1 Series
XX MPU product line in the series STM32MP157
Y
Security option:
A: basic security
C: Secure Boot and cryptography
Secure Boot and cryptography
EVZ Evaluation board configuration
EV1: with PMIC PMIC
The order code is mentioned on a sticker placed on the top side of the board.
STM32MP157A-EV1 STM32MP157C-EV1
Ordering information
DB3800 - Rev 2 page 3/7
arm
2Development environment
STM32 Arm Cortex MPUs are based on the Arm® Cortex®-A and Cortex®-M processors.
Note: Arm is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
2.1 System requirements
• Windows® OS (7, 8 and 10), Linux® 64-bit, or macOS®
USB Type-C to Type-A cable
USB Type-A to Micro-B cable
USB Type-A to Micro-AB cable
Note: macOS® is a trademark of Apple Inc. registered in the U.S. and other countries.
2.2 Development toolchains
• Keil® MDK-ARM (see note)
• IAR EWARM (see note)
GCC-based IDEs
• GCC
Note: On Windows® only.
2.3 Demonstration software
The STM32 MPU OpenSTLinux Distribution and STM32CubeMP1 base demonstration software is preloaded in
the microSD for easy demonstration of the device peripherals in standalone mode. The latest versions of the
demonstration source code and associated documentation can be downloaded from www.st.com.
STM32MP157A-EV1 STM32MP157C-EV1
Development environment
DB3800 - Rev 2 page 4/7
3Technology partners
NANYA
4-Gbit DDR3L, 16-bit, part number NT5CC256M16ER-EK
TOSHIBA
32-Gbit eMMC, part number THGBMNG5D1LBAIL
MICRON
SLC NAND 8Gb/8bits/8ECC/4K PS, part number MT29F8G08ABACAH4-ITS:C
MACRONIX
512-Mbit Quad-SPI NOR Flash memory device, part number MX25L51245G-XD
STM32MP157A-EV1 STM32MP157C-EV1
Technology partners
DB3800 - Rev 2 page 5/7
Revision history
Table 3. Document revision history
Date Version Changes
5-Feb-2019 1 Initial release.
26-Aug-2019 2 Updated ST PMIC in Features. Reorganized Ordering information.
STM32MP157A-EV1 STM32MP157C-EV1
DB3800 - Rev 2 page 6/7
IMPORTANT NOTICE – PLEASE READ CAREFULLY
STMicroelectronics NV and its subsidiaries (“ST”) reserve the right to make changes, corrections, enhancements, modifications, and improvements to ST
products and/or to this document at any time without notice. Purchasers should obtain the latest relevant information on ST products before placing orders. ST
products are sold pursuant to ST’s terms and conditions of sale in place at the time of order acknowledgement.
Purchasers are solely responsible for the choice, selection, and use of ST products and ST assumes no liability for application assistance or the design of
Purchasers’ products.
No license, express or implied, to any intellectual property right is granted by ST herein.
Resale of ST products with provisions different from the information set forth herein shall void any warranty granted by ST for such product.
ST and the ST logo are trademarks of ST. For additional information about ST trademarks, please refer to www.st.com/trademarks. All other product or service
names are the property of their respective owners.
Information in this document supersedes and replaces information previously supplied in any prior versions of this document.
© 2019 STMicroelectronics – All rights reserved
STM32MP157A-EV1 STM32MP157C-EV1
DB3800 - Rev 2 page 7/7