42330A-MCU-07/2014
USER GUIDE
Atmel-ICE
The Atmel-ICE Debugger
Atmel-ICE is a powerful development tool for debugging and programming
ARM
®
Cortex
®
-M based Atmel
®
SAM and Atmel AVR
®
microcontrollers with On-
Chip Debug capability.
It supports:
Programming and on-chip debugging of all Atmel AVR 32-bit
microcontrollers on both JTAG and aWire interfaces
Programming and on-chip debugging of all Atmel AVR XMEGA
®
family
devices on both JTAG and PDI 2-wire interfaces
Programming (JTAG and SPI) and debugging of all Atmel AVR 8-bit
microcontrollers with OCD support on either JTAG or debugWIRE interfaces
Programming and debugging of all Atmel SAM ARM Cortex-M based
microcontrollers on both SWD and JTAG interfaces
Programming (TPI) of all Atmel tinyAVR
®
8-bit microcontrollers with support
for this interface
Consult the supported devices list in the Atmel Studio User Guide for a full list of
devices and interfaces supported by this firmware release.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
2
Table of Contents
The Atmel-ICE Debugger
.............................................................
1
1.
Introduction
..............................................................................
4
1.1.
Introduction to the Atmel-ICE
...................................................
4
1.2.
Atmel-ICE Features
...............................................................
4
1.3.
System Requirements
............................................................
4
2.
Getting Started with the Atmel-ICE
.........................................
6
2.1.
Full Kit Contents
...................................................................
6
2.2.
Basic Kit Contents
.................................................................
6
2.3.
PCBA Kit Contents
................................................................
7
2.4.
Spare Parts Kits
....................................................................
7
2.5.
Kit Overview
.........................................................................
8
2.6.
Assembling the Atmel-ICE
......................................................
8
2.7.
Opening the Atmel-ICE
.........................................................
10
2.8.
Powering the Atmel-ICE
........................................................
12
2.9.
Connecting to the Host Computer
...........................................
12
2.10.
USB Driver Installation
.........................................................
12
2.10.1.
Windows
................................................................
12
3.
Connecting the Atmel-ICE
....................................................
13
3.1.
Overview: Connecting to AVR and SAM Target Devices
..............
13
3.2.
Connecting to a JTAG Target
.................................................
13
3.3.
Connecting to an aWire Target
...............................................
14
3.4.
Connecting to a PDI Target
...................................................
15
3.5.
Connecting to a debugWIRE Target
........................................
15
3.6.
Connecting to a SPI Target
...................................................
16
3.7.
Connecting to a TPI Target
....................................................
17
3.8.
Connecting to a SWD Target
.................................................
17
4.
On-Chip Debugging
..............................................................
19
4.1.
Introduction to On-Chip Debugging (OCD)
................................
19
4.2.
Physical Interfaces
...............................................................
19
4.2.1.
JTAG
.....................................................................
19
4.2.2.
aWire
....................................................................
21
4.2.3.
PDI Physical
...........................................................
22
4.2.4.
debugWIRE
............................................................
22
4.2.5.
SPI
.......................................................................
22
4.2.6.
TPI
.......................................................................
23
4.2.7.
SWD
.....................................................................
23
4.3.
Atmel OCD Implementations
..................................................
23
4.3.1.
Atmel AVR UC3 OCD (JTAG and aWire)
......................
23
4.3.2.
Atmel AVR XMEGA OCD (JTAG and PDI Physical)
........
24
4.3.3.
Atmel megaAVR OCD (JTAG)
....................................
24
4.3.4.
Atmel megaAVR / tinyAVR OCD (debugWIRE)
..............
24
4.3.5.
ARM Coresight Components
.....................................
24
5.
Hardware Description
............................................................
25
5.1.
LEDs
.................................................................................
25
5.2.
Rear Panel
.........................................................................
25
5.3.
Bottom Panel
......................................................................
25
5.4.
Architecture Description
........................................................
26
5.4.1.
Atmel-ICE Mainboard
...............................................
26
5.4.2.
Atmel-ICE Target Connectors
.....................................
27
5.4.3.
Atmel-ICE target Connectors Part Numbers
..................
27
6.
Software Integration
..............................................................
28
6.1.
Atmel Studio
.......................................................................
28
6.1.1.
Software Integration in Atmel Studio
............................
28
6.1.2.
Programming Options
...............................................
28
6.1.3.
Debug Options
........................................................
28
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
3
7.
Command Line Utility
............................................................
30
8.
Advanced Debugging Techniques
........................................
31
8.1.
Atmel AVR UC3 Targets
.......................................................
31
8.1.1.
EVTI / EVTO Usage
.................................................
31
8.2.
debugWIRE Targets
.............................................................
31
8.2.1.
Software Breakpoints
...............................................
31
9.
Special Considerations
.........................................................
32
9.1.
Atmel AVR XMEGA OCD
......................................................
32
9.2.
Atmel megaAVR OCD and debugWIRE OCD
............................
32
9.2.1.
Atmel megaAVR OCD (JTAG)
....................................
33
9.2.2.
debugWIRE OCD
....................................................
34
9.3.
Atmel AVR UC3 OCD
...........................................................
35
9.4.
SAM / Coresight OCD
..........................................................
35
10. Firmware Upgrade
................................................................
37
11. Release History and Known issues
......................................
38
11.1.
What's New
........................................................................
38
11.2.
Firmware Release History
.....................................................
38
11.2.1.
Atmel Studio 6.2
.....................................................
38
11.2.2.
Atmel Studio 6.2 (beta)2
...........................................
38
11.3.
Known Issues Concerning the Atmel-ICE
.................................
38
11.3.1.
Atmel AVR XMEGA OCD Specific Issues
.....................
38
11.3.2.
Atmel megaAVR OCD and Atmel tinyAVR OCD
Specific Issues
........................................................
38
11.4.
Device Support
...................................................................
38
12. Product Compliance
..............................................................
39
12.1.
RoHS and WEEE
................................................................
39
12.2.
CE and FCC
......................................................................
39
13. Document Revisions
.............................................................
40
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
4
1.
Introduction
1.1
Introduction to the Atmel-ICE
Atmel-ICE is a powerful development tool for debugging and programming ARM Cortex-M based Atmel SAM
and Atmel AVR microcontrollers with On-Chip Debug capability.
It supports:
Programming and on-chip debugging of all Atmel AVR UC3 microcontrollers on both JTAG and aWire
interfaces
Programming and on-chip debugging of all AVR XMEGA family devices on both JTAG and PDI 2-wire
interfaces
Programming (JTAG and SPI) and debugging of all AVR 8-bit microcontrollers with OCD support on both
JTAG or debugWIRE interfaces
Programming and debugging of all Atmel SAM ARM Cortex-M based microcontrollers on both SWD and
JTAG interfaces
Programming (TPI) of all Atmel tinyAVR 8-bit microcontrollers with support for this interface
1.2
Atmel-ICE Features
Fully compatible with Atmel Studio
Supports programming and debugging of all Atmel AVR UC3 32-bit microcontrollers
Supports programming and debugging of all 8-bit AVR XMEGA devices
Supports programming and debugging of all 8-bit Atmel megaAVR
®
and tinyAVR devices with OCD
Supports programming and debugging of all SAM ARM Cortex-M based microcontrollers
Target operating voltage range of 1.62V to 5.5V
Draws less than 3mA from target VTref when using debugWIRE interface and less than 1mA for all other
interfaces
Supports JTAG clock frequencies from 32kHz to 7.5MHz
Supports PDI clock frequencies from 32kHz to 7.5MHz
Supports debugWIRE baud rates from 4kbit/s to 0.5Mbit/s
Supports aWire baud rates from 7.5kbit/s to 7Mbit/s
Supports SPI clock frequencies from 8kHz to 5MHz
Supports SWD clock frequencies from 32kHz to 2MHz
USB 2.0 high-speed host interface
ITM serial trace capture at up to 3MB/s
Supports 10-pin 50-mil JTAG connector with both AVR and Cortex pinouts. The standard probe cable
supports AVR 6-pin ISP/PDI/TPI 100-mil headers as well as 10-pin 50-mil. An adapter is available to
support 6-pin 50-mil, 10-pin 100-mil and 20-pin 100-mil headers. Several kit options are available with
different cabling and adapters.
1.3
System Requirements
The Atmel-ICE unit requires that a front-end debugging environment Atmel Studio version 6.2 or later is
installed on your computer.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
5
The Atmel-ICE should be connected to the host computer using the USB cable provided, or a certified USB-
micro cable.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
6
2.
Getting Started with the Atmel-ICE
2.1
Full Kit Contents
The Atmel-ICE full kit contains these items:
Atmel-ICE unit
USB cable (1.8m, high-speed, micro-B)
Adapter board containing 50-mil AVR, 100-mil AVR/SAM and 100-mil 20-pin SAM adapters
IDC flat cable with 10-pin 50-mil connector and 6-pin 100-mil connector
50-mil 10-pin mini squid cable with 10 x 100-mil sockets
Figure 2-1. Atmel-ICE Full Kit Contents
2.2
Basic Kit Contents
The Atmel-ICE basic kit contains these items:
Atmel-ICE unit
USB cable (1.8m, high-speed, micro-B)
IDC flat cable with 10-pin 50-mil connector and 6-pin 100-mil connector
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
7
Figure 2-2. Atmel-ICE Basic Kit Contents
2.3
PCBA Kit Contents
The Atmel-ICE PCBA kit contains these items:
Atmel-ICE unit without plastic encaptulation
Figure 2-3. Atmel-ICE PCBA Kit Contents
2.4
Spare Parts Kits
The following spare parts kits are available:
Adapter kit
Cable kit
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
8
Figure 2-4. Atmel-ICE Adapter Kit Contents
Figure 2-5. Atmel-ICE Cable Kit Contents
2.5
Kit Overview
The Atmel-ICE kit options are shown diagrammatically here:
Figure 2-6. Atmel-ICE Kit Overview
PCBA
PCBA kit
basic kit
adapter kit
full kit
SAM
AVR
cable kit
2.6
Assembling the Atmel-ICE
The Atmel-ICE unit is shipped with no cables attached. Two cable options are provided in the full kit:
50-mil 10-pin IDC flat cable with 6-pin ISP and 10-pin connectors
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
9
50-mil 10-pin mini-squid cable with 10 x 100-mil sockets
Figure 2-7. Atmel-ICE Cables
For most purposes, the 50-mil 10-pin IDC flat cable can be used, connecting either natively to its 10-pin or 6-
pin connectors, or connecting via the adapter board. Three adapters are provided on one small PCBA. The
following adapters are included:
100-mil 10-pin JTAG/SWD adapter
100-mil 20-pin SAM JTAG/SWD adapter
50-mil 6-pin SPI/debugWIRE/PDI/aWire adapter
Figure 2-8. Atmel-ICE Adapters
Note
A 50-mil JTAG adapter has not been provided - this is because the 50-mil 10-pin IDC cable can
be used to connect directly to a 50-mil JTAG header. For the part number of the component used
for the 50-mil 10-pin connector, see
"Atmel-ICE target Connectors Part Numbers" on page 27
.
The 6-pin ISP/PDI header is included as part of the 10-pin IDC cable. This termination can be cut off if it is not
required.
To assemble your Atmel-ICE into its default configuration, connect the 10-pin 50-mil IDC cable to the unit as
shown below. Be sure to orient the cable so that the red wire (pin 1) on the cable aligns with the triangular
indicator on the blue belt of the enclosure. The cable should connect upwards from the unit. Be sure to connect
to the port corresponding to the pinout of your target - AVR or SAM.
Figure 2-9. Atmel-ICE Cable Connection
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
10
Figure 2-10. Atmel-ICE AVR Probe Connection
Figure 2-11. Atmel-ICE SAM Probe Connection
2.7
Opening the Atmel-ICE
Note
For normal operation, the Atmel-ICE unit must not be opened. Opening the unit is done at your
own risk. Anti-static precautions should be taken.
The Atmel-ICE enclosure consists of three separate plastic components - top cover, bottom cover and blue
belt - which are snapped together during assembly. To open the unit, simply insert a large flat screwdriver into
the openings in the blue belt, apply some inward pressure and twist gently. Repeat the process on the other
snapper holes, and the top cover will pop off.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
11
Figure 2-12. Opening the Atmel-ICE (1)
Figure 2-13. Opening the Atmel-ICE (2)
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
12
Figure 2-14. Opening the Atmel-ICE(3)
To close the unit again, simply align the top and bottom covers correctly, and press together firmly.
2.8
Powering the Atmel-ICE
The Atmel-ICE is powered by the USB bus voltage. It requires less than 100mA to operate, and can therefore
be powered through a USB hub. The power LED will illuminate when the unit is plugged in. When not
connected in an active programming or debugging session, the unit will enter low-power consumption mode to
preserve your computer's battery. The Atmel-ICE cannot be powered down - it should be unplugged when not
in use.
2.9
Connecting to the Host Computer
The Atmel-ICE communicates primarily using a standard HID interface, and does not require a special driver on
the host computer. To use the advanced data gateway functionality of the Atmel-ICE, be sure to install the USB
driver on the host computer. This is done automatically when installing the front-end software provided free by
Atmel. See
www.atmel.com
1
for further information or to download the latest front-end software.
The Atmel-ICE must be connected to an available USB port on the host computer using the USB cable
provided, or suitable USB certified micro cable. The Atmel-ICE contains a USB 2.0 compliant controller, and
can operate in both full-speed and high-speed modes. For best results, connect the Atmel-ICE directly to a
USB 2.0 compliant high-speed hub on the host computer using the cable provided.
2.10
USB Driver Installation
2.10.1
Windows
When installing the Atmel-ICE on a computer running Microsoft
®
Windows
®
, the USB driver is loaded when the
Atmel-ICE is first plugged in.
Note
Be sure to install the front-end software packages before plugging the unit in for the first time.
Once successfully installed, the Atmel-ICE will appear in the device manager as a "Human Interface Device".
1
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
13
3.
Connecting the Atmel-ICE
3.1
Overview: Connecting to AVR and SAM Target Devices
The Atmel-ICE probe has two 50-mil 10-pin JTAG connectors accessible on the front of the tool's enclosure.
Both connectors are directly electrically connected, but conform to two different pinouts - the AVR JTAG header
and the ARM Cortex Debug header. The connector should be selected based on the pinout of the target board,
and not the target MCU type - for example a SAM device mounted in a AVR STK600 stack should use the AVR
header.
Various cabling and adapters are available in the different Atmel-ICE kits. An overview of connection options is
shown.
Figure 3-1. Atmel-ICE Connection Options
6-pin 100-mil AVR ISP/
debugWIRE/PDI/aWire/
TPI header
10-pin 100-mil AVR
JTAG header
10-pin 50-mil AVR
JTAG header
SAM
AVR
20-pin 100-mil SAM
header
(for EVKs etc)
10-pin 100-mil
JTAG/SWD header
10-pin 50-mil JTAG/SWD
(Cortex debug header)
SAM
AVR
6-pin 50-mil AVR ISP/
debugWIRE/PDI/aWire/
TPI header
3.2
Connecting to a JTAG Target
The Atmel-ICE probe has two 50-mil 10-pin JTAG connectors accessible on the front of the tool's enclosure.
Both connectors are directly electrically connected, but conform to two different pinouts - the AVR JTAG header
and the ARM Cortex Debug header. The connector should be selected based on the pinout of the target board,
and not the target MCU type - for example a SAM device mounted in a AVR STK600 stack should use the AVR
header.
The recommended pinout for the 10-pin AVR JTAG connector is shown in
Figure 4-2, "AVR JTAG Header
Pinout" on page 20
.
The recommended pinout for the 10-pin ARM Cortex Debug connector is shown in
Figure 4-3, "SAM JTAG
Header Pinout" on page 20
.
Direct connection to a standard 10-pin 50-mil header
Use the 50-mil 10-pin flat cable (included in some kits) to connect directly to a board supporting this header
type. Use the AVR connector port on the Atmel-ICE for headers layed out in the AVR pinout, and the SAM
connector port for headers complying with the ARM Cortex Debug header pinout.
The pinouts for both 10-pin connector ports are shown below.
Connection to a standard 10-pin 100-mil header
Use a standard 50-mil to 100-mil adapter to connect to 100-mil headers. An adapter board (included in some
kits) can be used for this purpose, or alternatively the JTAGICE3 adapter can be used for AVR targets.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
14
Note
The JTAGICE3 100-mil adapter cannot be used with the SAM connector port, since pins 2 and 10
(AVR GND) on the adapter are connected.
Connection to a custom 100-mil header
If your target board does not have a compliant 10-pin JTAG header in 50- or 100-mil, you can map to a custom
pinout using the 10-pin "mini-squid" cable (included in some kits), which gives access to ten individual 100-mil
sockets.
Connection to a 20-pin 100-mil header
Use the adapter board (included in some kits) to connect to targets with a 20-pin 100-mil header.
Table 3-1. Atmel-ICE JTAG Pin Description
Name
AVR
port
pin
SAM
port
pin
Description
TCK
1
4
Test Clock (clock signal from the Atmel-ICE into the target device).
TMS
5
2
Test Mode Select (control signal from the Atmel-ICE into the target device).
TDI
9
8
Test Data In (data transmitted from the Atmel-ICE into the target device).
TDO
3
6
Test Data Out (data transmitted from the target device into the Atmel-ICE).
nTRST
8
-
Test Reset (optional, only on some AVR devices). Used to reset the JTAG
TAP controller.
nSRST
6
10
Reset (optional) Used to reset the target device. Connecting this pin is
recommended since it allows the Atmel-ICE to hold the target device in a
reset state, which can be essential to debugging in certain scenarios.
VTG
4
1
Target voltage reference. The Atmel-ICE samples the target voltage on this
pin in order to power the level converters correctly. The Atmel-ICE draws
less than 3mA from this pin in debugWIRE mode and less than 1mA in other
modes.
GND
2, 10
3, 5, 9
Ground. All must be connected to ensure that the Atmel-ICE and the target
device share the same ground reference.
3.3
Connecting to an aWire Target
The aWire interface only requires one data line in addition to Vcc and GND. On the target this line is the
nRESET line, although the debugger uses the JTAG TDO line as the data line.
The recommended pinout for the 6-pin aWire connector is shown in
Figure 4-5, "aWire Header
Pinout" on page 22
.
Connection to a 6-pin 100-mil aWire header
Use the 6-pin 100-mil tap on the flat cable (included in some kits) to connect to a standard 100-mil aWire
header.
Connection to a 6-pin 50-mil aWire header
Use the adapter board (included in some kits) to connect to a standard 50-mil aWire header.
Connection to a custom 100-mil header
The 10-pin mini-squid cable should be used to connect between the Atmel-ICE AVR connector port and the
target board. Three connections are required, as described in the table below.
Table 3-2. Atmel-ICE aWire Pin Mapping
Atmel-ICE AVR port
pins
Target pins
Mini-squid pin
aWire pinout
Pin 1 (TCK)
1
Pin 2 (GND)
GND
2
6
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
15
Atmel-ICE AVR port
pins
Target pins
Mini-squid pin
aWire pinout
Pin 3 (TDO)
DATA
3
1
Pin 4 (VTG)
VTG
4
2
Pin 5 (TMS)
5
Pin 6 (nSRST)
6
Pin 7 (Not connected)
7
Pin 8 (nTRST)
8
Pin 9 (TDI)
9
Pin 10 (GND)
0
3.4
Connecting to a PDI Target
The recommended pinout for the 6-pin PDI connector is shown in
Figure 4-6, "PDI Header
Pinout" on page 22
.
Connection to a 6-pin 100-mil PDI header
Use the 6-pin 100-mil tap on the flat cable (included in some kits) to connect to a standard 100-mil PDI header.
Connection to a 6-pin 50-mil PDI header
Use the adapter board (included in some kits) to connect to a standard 50-mil PDI header.
Connection to a custom 100-mil header
The 10-pin mini-squid cable should be used to connect between the Atmel-ICE AVR connector port and the
target board. Four connections are required, as described in the table below.
Note
There is a difference from the JTAGICE mkII JTAG probe, where PDI_DATA is connected to pin 9.
The Atmel-ICE is compatible with the pinout used by the JTAGICE3, AVR ONE! and AVR Dragon
products.
Table 3-3. Atmel-ICE PDI Pin Mapping
Atmel-ICE AVR port
pin
Target pins
Mini-squid pin
Atmel STK600 PDI
pinout
Pin 1 (TCK)
1
Pin 2 (GND)
GND
2
6
Pin 3 (TDO)
PDI_DATA
3
1
Pin 4 (VTG)
VTG
4
2
Pin 5 (TMS)
5
Pin 6 (nSRST)
PDI_CLK
6
5
Pin 7 (Not connected)
7
Pin 8 (nTRST)
8
Pin 9 (TDI)
9
Pin 10 (GND)
0
3.5
Connecting to a debugWIRE Target
The recommended pinout for the 6-pin debugWIRE (SPI) connector is shown in
Figure 4-7, "debugWIRE (SPI)
Header Pinout" on page 22
.
Connection to a 6-pin 100-mil SPI header
Use the 6-pin 100-mil tap on the flat cable (included in some kits) to connect to a standard 100-mil SPI header.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
16
Connection to a 6-pin 50-mil SPI header
Use the adapter board (included in some kits) to connect to a standard 50-mil SPI header.
Connection to a custom 100-mil header
The 10-pin mini-squid cable should be used to connect between the Atmel-ICE AVR connector port and
the target board. Three connections are required, as described in
Table 3-4, "Atmel-ICE debugWIRE Pin
Mapping" on page 16
.
Although the debugWIRE interface only requires one signal line (RESET), Vcc and GND to operate correctly,
it is advised to have access to the full SPI connector so that the debugWIRE interface can be enabled and
disabled using SPI programming.
When the DWEN fuse is enabled the SPI interface is overridden internally in order for the OCD module to have
control over the RESET pin. The debugWIRE OCD is capable of disabling itself temporarily (using the button
on the debugging tab in the properties dialog in Atmel Studio), thus releasing control of the RESET line. The
SPI interface is then available again (only if the SPIEN fuse is programmed), allowing the DWEN fuse to be
un-programmed using the SPI interface. If power is toggled before the DWEN fuse is un-programmed, the
debugWIRE module will again take control of the RESET pin.
Note
It is highly advised to simply let Atmel Studio handle setting and clearing of the DWEN fuse.
It is not possible to use the debugWIRE interface if the lockbits on the target AVR device are programmed.
Always be sure that the lockbits are cleared before programming the DWEN fuse and never set the lockbits
while the DWEN fuse is programmed. If both the debugWIRE enable fuse (DWEN) and lockbits are set,
one can use High Voltage Programming to do a chip erase, and thus clear the lockbits. When the lockbits
are cleared the debugWIRE interface will be re-enabled. The SPI Interface is only capable of reading fuses,
reading signature and performing a chip erase when the DWEN fuse is un-programmed.
Table 3-4. Atmel-ICE debugWIRE Pin Mapping
Atmel-ICE AVR port pin
Target pins
Mini-squid pin
Pin 1 (TCK)
1
Pin 2 (GND)
GND
2
Pin 3 (TDO)
3
Pin 4 (VTG)
VTG
4
Pin 5 (TMS)
5
Pin 6 (nSRST)
RESET
6
Pin 7 (Not connected)
7
Pin 8 (nTRST)
8
Pin 9 (TDI)
9
Pin 10 (GND)
0
3.6
Connecting to a SPI Target
The recommended pinout for the 6-pin SPI connector is shown in
Figure 4-8, "SPI Header
Pinout" on page 23
.
Connection to a 6-pin 100-mil SPI header
Use the 6-pin 100-mil tap on the flat cable (included in some kits) to connect to a standard 100-mil SPI header.
Connection to a 6-pin 50-mil SPI header
Use the adapter board (included in some kits) to connect to a standard 50-mil SPI header.
Connection to a custom 100-mil header
The 10-pin mini-squid cable should be used to connect between the Atmel-ICE AVR connector port and the
target board. Six connections are required, as described in the table below.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
17
Note
The SPI interface is effectively disabled when the debugWIRE enable fuse (DWEN) is
programmed, even if SPIEN fuse is also programmed. To re-enable the SPI interface, the 'disable
debugWIRE' command must be issued while in a debugWIRE debugging session. Disabling
debugWIRE in this manner requires that the SPIEN fuse is already programmed. If Atmel Studio
fails to disable debugWIRE, it is probable that the SPIEN fuse is NOT programmed. If this is the
case, it is necessary to use a high-voltage programming interface to program the SPIEN fuse.
Table 3-5. Atmel-ICE SPI Pin Mapping
Atmel-ICE AVR port
pins
Target pins
Mini-squid pin
SPI pinout
Pin 1 (TCK)
SCK
1
3
Pin 2 (GND)
GND
2
6
Pin 3 (TDO)
MISO
3
1
Pin 4 (VTG)
VTG
4
2
Pin 5 (TMS)
5
Pin 6 (nSRST)
/RESET
6
5
Pin 7 (Not connected)
7
Pin 8 (nTRST)
8
Pin 9 (TDI)
MOSI
9
4
Pin 10 (GND)
0
3.7
Connecting to a TPI Target
The recommended pinout for the 6-pin TPI connector is shown in
Figure 4-9, "TPI Header
Pinout" on page 23
.
Connection to a 6-pin 100-mil TPI header
Use the 6-pin 100-mil tap on the flat cable (included in some kits) to connect to a standard 100-mil TPI header.
Connection to a 6-pin 50-mil TPI header
Use the adapter board (included in some kits) to connect to a standard 50-mil TPI header.
Connection to a custom 100-mil header
The 10-pin mini-squid cable should be used to connect between the Atmel-ICE AVR connector port
and the target board. Six connections are required, as described in
Table 3-6, "Atmel-ICE TPI Pin
Mapping" on page 17
.
Table 3-6. Atmel-ICE TPI Pin Mapping
Atmel-ICE AVR port
pins
Target pins
Mini-squid pin
TPI pinout
Pin 1 (TCK)
CLOCK
1
3
Pin 2 (GND)
GND
2
6
Pin 3 (TDO)
DATA
3
1
Pin 4 (VTG)
VTG
4
2
Pin 5 (TMS)
5
Pin 6 (nSRST)
/RESET
6
5
Pin 7 (Not connected)
7
Pin 8 (nTRST)
8
Pin 9 (TDI)
9
Pin 10 (GND)
0
3.8
Connecting to a SWD Target
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
18
The ARM SWD interface is s subset of the JTAG interface, making use of TCK and TMS pins, which means
that when connecting to an SWD device, the 10-pin JTAG connector can technically be used. The ARM JTAG
and AVR JTAG connectors are however not pin-compatible, so this depends upon the layout of the target board
in use. When using STK600 or a board making use of the AVR JTAG pinout, the AVR connector port on the
Atmel-ICE must be used. When connecting to a board which makes use of the ARM JTAG pinout, the SAM
connector port on the Atmel-ICE must be used.
The recommended pinout for the 10-pin Cortex Debug connector is shown in
Figure 4-10, "Recommended
ARM SWD/JTAG Header Pinout" on page 23
.
Connection to a 10-pin 50-mil Cortex header
Use the flat cable (included in some kits) to connect to a standard 50-mil Cortex header.
Connection to a 10-pin 100-mil Cortex-layout header
Use the adapter board (included in some kits) to connect to a 100-mil Cortex-pinout header.
Connection to a 20-pin 100-mil SAM header
Use the adapter board (included in some kits) to connect to a 20-pin 100-mil SAM header.
Connection to a custom 100-mil header
The 10-pin mini-squid cable should be used to connect between the Atmel-ICE AVR or SAM connector port
and the target board. Six connections are required, as described in the table below.
Table 3-7. Atmel-ICE SWD Pin Mapping
Name
AVR
port
pin
SAM
port
pin
Description
SWDCLK 1
4
Serial Wire Debug Clock.
SWDIO
5
2
Serial Wire Debug Data Input/Output.
SWO
3
6
Serial Wire Output (optional- not implemented on all devices).
nSRST
6
10
Reset.
VTG
4
1
Target voltage reference.
GND
2, 10
3, 5
Ground.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
19
4.
On-Chip Debugging
4.1
Introduction to On-Chip Debugging (OCD)
A traditional
Emulator
is a tool which tries to imitate the exact behaviour of a target device. The closer this
behaviour is to the actual device's behaviour, the better the emulation will be.
The Atmel-ICE is not a traditional
Emulator
. Instead, the Atmel-ICE interfaces with the internal On-Chip Debug
system inside the target device, providing a mechanism for monitoring and controlling its execution. In this way
the application being debugged is not
emulated
, but actually executed on the real target device.
With an OCD system, the application can be executed whilst maintaining exact electrical and timing
characteristics in the target system – something not technically realisable with a traditional
emulator
.
Run Mode
When in Run mode, the execution of code is completely independent of the Atmel-ICE. The Atmel-ICE will
continuously monitor the target device to see if a break condition has occurred. When this happens the OCD
system will interrogate the device through its debug interface, allowing the user to view the internal state of the
device.
Stopped Mode
When a breakpoint is reached, program execution is halted, but all I/O will continue to run as if no breakpoint
had occurred. For example assume that a USART transmit has just been initiated when a breakpoint is
reached. In this case the USART continues to run at full speed completing the transmission, even though the
core is in stopped mode.
Hardware Breakpoints
The target OCD module contains a number of program counter comparators implemented in hardware. When
the program counter matches the value stored in one of the comparator registers, the OCD enters stopped
mode. Since hardware breakpoints require dedicated hardware on the OCD module, the number of breakpoints
available depends upon the size of the OCD module implemented on the target. Usually one such hardware
comparator is 'reserved'' by the debugger for internal use. For more information on the hardware breakpoints
available in the various OCD modules, see
"Atmel OCD Implementations" on page 23
.
Software Breakpoints
A software breakpoint is a BREAK instruction placed in program memory on the target device. When this
instruction is loaded, program execution will break and the OCD enters stopped mode. To continue execution
a "start" command has to be given from the OCD. Not all AVR devices have OCD modules supporting the
BREAK instruction. For more information on the software breakpoints available in the various OCD modules,
see
"Atmel OCD Implementations" on page 23
.
For further information on the considerations and restrictions when using an OCD system, see
"Special
Considerations" on page 32
.
4.2
Physical Interfaces
The Atmel-ICE supports several hardware interfaces as described in the following sections.
4.2.1
JTAG
The JTAG interface consists of a 4-wire Test Access Port (TAP) controller that is compliant with the IEEE
1149.1 standard. The IEEE standard was developed to provide an industry-standard way to efficiently test
circuit board connectivity (Boundary Scan). Atmel AVR and SAM devices have extended this functionality to
include full Programming and On-Chip Debugging support.
Figure 4-1. JTAG Interface Basics
Atmel
target device
Atmel-ICE
Vcc
TMS
TDI
TDO
TCK
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
20
When designing an application PCB which includes an Atmel AVR with the JTAG interface, it is recommended
to use the pinout as shown in
Figure 4-2, "AVR JTAG Header Pinout" on page 20
. The Atmel-ICE can
connect to both 100-mil and 50-mil variants of this pinout.
Figure 4-2. AVR JTAG Header Pinout
GND
VCC
/RESET
(TRST)
GND
TCK
TDO
TMS
TDI
1
2
AVR JTAG
(NC)
Table 4-1. AVR JTAG Pin Description
Name
Pin
Description
TCK
1
Test Clock (clock signal from the Atmel-ICE into the target device).
TMS
5
Test Mode Select (control signal from the Atmel-ICE into the target device).
TDI
9
Test Data In (data transmitted from the Atmel-ICE into the target device).
TDO
3
Test Data Out (data transmitted from the target device into the Atmel-ICE).
nTRST
8
Test Reset (optional, only on some AVR devices). Used to reset the JTAG TAP
controller.
nSRST
6
Reset (optional) Used to reset the target device. Connecting this pin is recommended
since it allows the Atmel-ICE to hold the target device in a reset state, which can be
essential to debugging in certain scenarios.
VTG
4
Target voltage reference. The Atmel-ICE samples the target voltage on this pin in
order to power the level converters correctly. The Atmel-ICE draws less than 3mA
from this pin in debugWIRE mode and less than 1mA in other modes.
GND
2, 10
Ground. Both must be connected to ensure that the Atmel-ICE and the target device
share the same ground reference.
Tip
Remember to include a decoupling capacitor between pin 4 and GND.
When designing an application PCB which includes an Atmel SAM with the JTAG interface, it is recommended
to use the pinout as shown in
Figure 4-3, "SAM JTAG Header Pinout" on page 20
. The Atmel-ICE can
connect to both 100-mil and 50-mil variants of this pinout.
Figure 4-3. SAM JTAG Header Pinout
TMS
TCK
TDO
TDI
nRESET
VCC
GND
GND
(KEY)
GND
1
2
SAM JTAG
Table 4-2. SAM JTAG pin description
Name
Pin
Description
TCK
4
Test Clock (clock signal from the Atmel-ICE into the target device).
TMS
3
Test Mode Select (control signal from the Atmel-ICE into the target device).
TDI
8
Test Data In (data transmitted from the Atmel-ICE into the target device).
TDO
6
Test Data Out (data transmitted from the target device into the Atmel-ICE).
nRESET
10
Reset (optional) Used to reset the target device. Connecting this pin is recommended
since it allows the Atmel-ICE to hold the target device in a reset state, which can be
essential to debugging in certain scenarios.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
21
Name
Pin
Description
VTG
1
Target voltage reference. The Atmel-ICE samples the target voltage on this pin in
order to power the level converters correctly. The Atmel-ICE draws less than 3mA
from this pin in debugWIRE mode and less than 1mA in other modes.
GND
3, 5, 9
Ground. All must be connected to ensure that the Atmel-ICE and the target device
share the same ground reference.
KEY
7
Connected internally to TRST pin on the AVR connector. Recommended as not
connected.
Tip
Remember to include a decoupling capacitor between pin 4 and GND.
The JTAG interface allows for several devices to be connected to a single interface in a daisy-chain
configuration. The target devices must all be powered by the same supply voltage, share a common ground
node, and must be connected as shown in
Figure 4-4, "JTAG Daisy-Chain" on page 21
.
Figure 4-4. JTAG Daisy-Chain
target
device
1
Atmel-ICE
TMS
TDI
TDO
TCK
target
device
2
target
device
3
When connecting devices in a daisy-chain, the following points must be considered:
All devices must share a common ground, connected to GND on the Atmel-ICE probe
All devices must be operating on the same target voltage. VTG on the Atmel-ICE must be connected to this
voltage
TMS and TCK are connected in parallel; TDI and TDO are connected in a serial chain
nSRST on the Atmel-ICE probe must be connected to RESET on the devices if any one of the devices in
the chain disables its JTAG port
"Devices before" refers to the number of JTAG devices that the TDI signal has to pass through in the daisy
chain before reaching the target device. Similarly "devices after" is the number of devices that the signal
has to pass through after the target device before reaching the Atmel-ICE TDO pin
"Instruction bits before" and "after" refers to the sum total of all JTAG devices' instruction register lengths
which are connected before and after the target device in the daisy chain
The total IR length (instruction bits before + Atmel AVR IR length + instruction bits after) is limited to a
maximum of 256 bits. The number of devices in the chain is limited to 15 before and 15 after
Tip
Daisy chaining example: TDI → ATmega1280 → ATxmega128A1 → ATUC3A0512 → TDO
In order to connect to the Atmel AVR XMEGA device, the daisy chain settings are:
Devices before: 1
Devices after: 1
Instruction bits before: 4 (8-bit AVR devices have 4 IR bits)
Instruction bits after: 5 (32-bit AVR devices have 5 IR bits)
4.2.2
aWire
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
22
The aWire interface makes use the RESET wire of the AVR device to allow programming and debugging
functions. A special enable sequence is transmitted by the Atmel-ICE which disables the default RESET
functionality of the pin.
When designing an application PCB which includes an Atmel AVR with the aWire interface, it is recommended
to use the pinout as shown in
Figure 4-5, "aWire Header Pinout" on page 22
. The Atmel-ICE ships with both
100-mil and 50-mil adapters supporting this pinout.
Figure 4-5. aWire Header Pinout
(RESET_N) DATA
VCC
GND
1
2
aWire
(NC)
(NC)
(NC)
Tip
Since aWire is a half-duplex interface, a pull-up resistor on the RESET line in the order of 47k is
recommended to avoid false start-bit detection when changing direction.
The aWire interface can be used as both a programming and debugging interface, all features of the OCD
system available through the 10-pin JTAG interface can also be accessed using aWire.
4.2.3
PDI Physical
The Program and Debug Interface (PDI) is an Atmel proprietary interface for external programming and on-
chip debugging of a device. PDI Physical is a 2-pin interface providing a bi-directional half-duplex synchronous
communication with the target device.
When designing an application PCB which includes an Atmel AVR with the PDI interface, the pinout shown in
Figure 4-6, "PDI Header Pinout" on page 22
should be used. One of the 6-pin adapters provided with the
Atmel-ICE kit can then be used to connect the Atmel-ICE probe to the application PCB.
Figure 4-6. PDI Header Pinout
PDI_DATA
PDI_CLK
VCC
GND
1
2
PDI
(NC)
(NC)
4.2.4
debugWIRE
The debugWIRE interface was developed by Atmel for use on low pin-count devices. Unlike the JTAG interface
which uses four pins, debugWIRE makes use of just a single pin (RESET) for bi-directional half-duplex
asynchronous communication with the debugger tool.
When designing an application PCB which includes an Atmel AVR with the debugWIRE interface, the pinout
shown in
Figure 4-7, "debugWIRE (SPI) Header Pinout" on page 22
should be used.
Figure 4-7. debugWIRE (SPI) Header Pinout
PDO/MISO
SCK
/RESET
VCC
PDI/MOSI
GND
1
2
SPI
Note
The debugWIRE interface can not be used as a programming interface. This means that the SPI
interface must also be available (as shown in
Figure 4-8, "SPI Header Pinout" on page 23
) in
order to program the target.
When the debugWIRE enable (DWEN) fuse is programmed and lock-bits are un-programmed, the debugWIRE
system within the target device is activated. The RESET pin is configured as a wire-AND (open-drain)
bi-directional I/O pin with pull-up enabled and becomes the communication gateway between target and
debugger.
4.2.5
SPI
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
23
In-System Programming uses the target Atmel AVR's internal SPI (Serial Peripheral Interface) to
download code into the flash and EEPROM memories. It is not a debugging interface. When designing an
application PCB which includes an AVR with the SPI interface, the pinout shown in
Figure 4-8, "SPI Header
Pinout" on page 23
should be used.
Figure 4-8. SPI Header Pinout
PDO/MISO
SCK
/RESET
VCC
PDI/MOSI
GND
1
2
SPI
4.2.6
TPI
TPI is a programming-only interface for some AVR ATtiny devices. It is not a debugging interface, and these
devices to not have OCD capability. When designing an application PCB which includes an AVR with the TPI
interface, the pinout shown in
Figure 4-9, "TPI Header Pinout" on page 23
should be used.
Figure 4-9. TPI Header Pinout
TPIDATA
TPICLK
/RESET
VCC
GND
1
2
TPI
(NC)
4.2.7
SWD
The ARM SWD interface is a subset of the JTAG interface, making use of TCK and TMS pins. The ARM JTAG
and AVR JTAG connectors are however not pin-compatible, so when designing an application PCB which uses
a SAM device with SWD or JTAG interface, it is recommended to use the ARM pinout shown in
Figure 4-10,
"Recommended ARM SWD/JTAG Header Pinout" on page 23
. The SAM connector port on the Atmel-ICE
can connect directly to this pinout.
Figure 4-10. Recommended ARM SWD/JTAG Header Pinout
SWDIO
SWDCLK
SWO
nRESET
VCC
GND
GND
(KEY)
GND
1
2
SAM SWD
(NC)
The Atmel-ICE is capable of streaming UART-format ITM trace to the host computer. Trace is captured on the
TRACE/SWO pin of the 10-pin header (JTAG TDO pin). Data is buffered internally on the Atmel-ICE and is sent
over the HID interface to the host computer. The maximum reliable data rate is about 3MB/s.
4.3
Atmel OCD Implementations
4.3.1
Atmel AVR UC3 OCD (JTAG and aWire)
The Atmel AVR UC3 OCD system is designed in accordance with the Nexus 2.0 standard (IEEE-ISTO
5001™-2003), which is a highly flexible and powerful open on-chip debug standard for 32-bit microcontrollers.
It supports the following features:
Nexus compliant debug solution
OCD supports any CPU speed
Six program counter hardware breakpoints
Two data breakpoints
Breakpoints can be configured as watchpoints
Hardware breakpoints can be combined to give break on ranges
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
24
Unlimited number of user program breakpoints (using BREAK)
Real-time program counter branch tracing, data trace, process trace (not supported by Atmel-ICE)
For special considerations regarding this debug interface, see
"Atmel AVR UC3 OCD" on page 35
.
For more information regarding the UC3 OCD system, consult the AVR32UC Technical Reference Manuals,
located on
www.atmel.com/uc3
1
.
4.3.2
Atmel AVR XMEGA OCD (JTAG and PDI Physical)
The Atmel AVR XMEGA OCD is otherwise known as PDI (Program and Debug Interface). Two physical
interfaces (JTAG and PDI physical) provide access to the same OCD implementation within the device. It
supports the following features:
Complete program flow control
One dedicated program address comparator or symbolic breakpoint (reserved)
Four hardware comparators
Unlimited number of user program breakpoints (using BREAK)
No limitation on system clock frequency
For special considerations regarding this debug interface, see
"Special Considerations" on page 32
.
4.3.3
Atmel megaAVR OCD (JTAG)
The Atmel megaAVR OCD is based on the JTAG physical interface. It supports the following features:
Complete program flow control
Four program memory (hardware) breakpoints (one is reserved)
Hardware breakpoints can be combined to form data breakpoints
Unlimited number of program breakpoints (using BREAK) (except ATmega128[A])
For special considerations regarding this debug interface, see
"Atmel megaAVR OCD (JTAG)" on page 33
.
4.3.4
Atmel megaAVR / tinyAVR OCD (debugWIRE)
The debugWIRE OCD is a specialised OCD module with a limited feature set specially designed for Atmel AVR
devices with low pin-count. It supports the following features:
Complete program flow control
Unlimited Number of User Program Breakpoints (using BREAK)
Automatic baud configuration based on target clock
For special considerations regarding this debug interface, see
"Atmel megaAVR OCD (JTAG)" on page 33
.
4.3.5
ARM Coresight Components
Atmel ARM Cortex-M based microcontrollers implement Coresight™ compliant OCD components. The features
of these components can vary from device to device. For further information consult the device's datasheet.
1
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
25
5.
Hardware Description
5.1
LEDs
The Atmel-ICE top panel has three LEDs which indicate the status of current debug or programming sessions.
Table 5-1. LEDs
LED
Function
Description
Left
Target power
GREEN when target power is OK. Flashing indicates a target power
error. Does not light up until a programming/debugging session
connection is started.
Middle
Main power
RED when main-board power is OK.
Right
Status
GREEN when the target is running. ORANGE when target is
stopped.
5.2
Rear Panel
The rear panel of the Atmel-ICE houses the micro-B USB connector.
5.3
Bottom Panel
The bottom panel of the Atmel-ICE has a sticker which shows the serial number and date of manufacture.
When seeking technical support, include these details.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
26
5.4
Architecture Description
The Atmel-ICE architecture is shown in the block diagram in
Figure 5-1, "Atmel-ICE block
diagram" on page 26
.
Figure 5-1. Atmel-ICE block diagram
5.4.1
Atmel-ICE Mainboard
Power is supplied to the Atmel-ICE from the USB bus, regulated to 3.3V by a step-down switchmode regulator.
The VTG pin is used as a reference input only, and a separate power supply feeds the variable-voltage side of
the on-board level converters At the heart of the Atmel-ICE mainboard is the Atmel AVR UC3 microcontroller
AT32UC3A4256, which runs at between 1MHz and 60MHz depending on the tasks being processed. The
microcontroller includes an on-chip USB 2.0 high-speed module, allowing high data throughput to and from the
debugger.
Communication between the Atmel-ICE and the target device is done through a bank of level converters that
shift signals between the target's operating voltage and the internal voltage level on the Atmel-ICE. Also in
the signal path are zener overvoltage protection diodes, series termination resistors, inductive filters and ESD
protection diodes. All signal channels can be operated in the range 1.62V to 5.5V, although the Atmel-ICE
hardware can not drive out a higher voltage than 5.0V. Maximum operating frequency varies according to the
target interface in use.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
27
5.4.2
Atmel-ICE Target Connectors
The Atmel-ICE does not have an active probe. A 50-mil IDC cable is used to connect to the target application
either directly, or through the adapters included in some kits. For more information on the cabling and adapters,
see section
Assembling the Atmel-ICE
5.4.3
Atmel-ICE target Connectors Part Numbers
In order to connect the Atmel-ICE 50-mil IDC cable directly to a target board, any standard 50-mil 10-pin
header should suffice. It is advised to use keyed headers to ensure correct orientation when connecting to the
target, such as those used on the adapter board included with the kit.
The part number for this header is: FTSH-105-01-L-DV-K-A-P from SAMTEC.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
28
6.
Software Integration
6.1
Atmel Studio
6.1.1
Software Integration in Atmel Studio
Atmel Studio is an Integrated Development Environment (IDE) for writing and debugging Atmel AVR and Atmel
SAM applications in Windows environments. Atmel Studio provides a project management tool, source file
editor, simulator, assembler and front-end for C/C++, programming, emulation and on-chip debugging.
Atmel Studio version 6.2 or later must be used in conjunction with the Atmel-ICE.
6.1.2
Programming Options
Atmel Studio supports programming of Atmel AVR and Atmel SAM ARM devices using the Atmel-ICE. The
programming dialog can be configured to use JTAG, aWire, SPI, PDI, TPI or SWD modes, according to the
target device selected.
When configuring the clock frequency, different rules apply for different interfaces and target families:
SPI programming makes use of the target clock. Configure the clock frequency to be lower than one fourth
the frequency at which the target device is currently running
JTAG programming on Atmel megaAVR devices is clocked by the programmer. This means that the
programming clock frequency is limited to the maximum operating frequency of the device itself. (Usually
16MHz)
AVR XMEGA programming on both JTAG and PDI interfaces is clocked by the programmer. This means
that the programming clock frequency is limited to the maximum operating frequency of the device itself.
(Usually 32MHz)
AVR UC3 programming on JTAG interface is clocked by the programmer. This means that the
programming clock frequency is limited to the maximum operating frequency of the device itself. (Limited to
33MHz)
AVR UC3 programming on aWire interface is clocked by the programmer. The optimal frequency is given
by the SAB bus speed in the target device. The Atmel-ICE debugger will automatically tune the aWire baud
rate to meet this criteria. Although it's usually not necessary the user can limit the maximum baud rate if
needed (e.g. in noisy environments)
SAM device programming on SWD interface is clocked by the programmer. The maximum frequency
supported by Atmel-ICE is 2MHz. The frequency should not exceed the target CPU frequency times 10,
.
6.1.3
Debug Options
When debugging an Atmel AVR device using Atmel Studio, the 'Tool' tab in the project properties view contains
some important configuration options. Those options which need further explanation are:
Target Clock Frequency
Accurately setting the target clock frequency is vital to achieve reliable debugging of Atmel megaAVR
device over the JTAG interface. This setting should be less than one fourth of the lowest operating
frequency of your AVR target device in the application being debugged. See
"Atmel megaAVR OCD
(JTAG)" on page 33
for more information.
Debug sessions on debugWIRE target devices are clocked by the target device itself, and thus
no frequency setting is required. The Atmel-ICE will automatically select the correct baud rate for
communicating at the start of a debug session. However, if you are experiencing reliability problems
related to a noisy debug environment, it is possible to force the debugWIRE speed to a fraction of its
"recommended" setting.
Debug sessions on AVR XMEGA target devices can be clocked at up to the maximum speed of the device
itself (usually 32MHz).
Debug sessions on AVR UC3 target devices over the JTAG interface can be clocked at up to the maximum
speed of the device itself (limited to 33MHz). However the optimal frequency will be slightly below the
current SAB clock on the target device.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
29
Debug sessions on UC3 target devices over the aWire interface will be automatically tuned to the optimal
baud rate by the Atmel-ICE itself. However, if you are experiencing reliability problems related to a noisy
debug environment, it is possible to force the aWire speed below a configurable limit.
Debug sessions on SAM target devices over the SWD interface can be clocked at up to ten times the CPU
clock (but limited to 2MHz max).
Preserve EEPROM
Select this option to avoid erasing the EEPROM during reprogramming of the target before a debug
session.
Use external reset
If your target application disables the JTAG interface, the external reset must be pulled low during
programming. Selecting this option avoids repeatedly being asked whether to use the external reset.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
30
7.
Command Line Utility
Atmel Studio comes with a command line utility called atprogram that can be used to program targets using
the Atmel Atmel-ICE. During the Atmel Studio installation a shortcut called Atmel Studio 6.2 Command Prompt
were created in the Atmel folder on the Start menu. By double clicking this shortcut a command prompt will be
opened and programming commands can be entered. The command line utility is installed in the Atmel Studio
installation path in the folder Atmel/Atmel Studio 6.2/atbackend/.
To get more help on the command line utility type the command:
atprogram --help
.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
31
8.
Advanced Debugging Techniques
8.1
Atmel AVR UC3 Targets
8.1.1
EVTI / EVTO Usage
The EVTI and EVTO pins are not accessible on the Atmel-ICE. However, they can still be used in conjunction
with other external equipment.
EVTI can be used for the following purposes:
The target can be forced to stop execution in response to an external event. If the Event In Control (EIC)
bits in the DC register are written to
0b01
, high-to-low transition on the EVTI pin will generate a breakpoint
condition. EVTI must remain low for one CPU clock cycle to guarantee that a breakpoint is triggered. The
External Breakpoint bit (EXB) in DS is set when this occurs
Generating trace synchronisation messages. Not used by the Atmel-ICE
EVTO can be used for the following purposes:
Indicating that the CPU has entered debug mode. Setting the EOS bits in DC to
0b01
causes the EVTO
pin to be pulled low for one CPU clock cycle when the target device enters debug mode. This signal can be
used as a trigger source for an external oscilloscope
Indicating that the CPU has reached a breakpoint or watchpoint. By setting the EOC bit in a corresponding
Breakpoint / Watchpoint Control Register, breakpoint or watchpoint status is indicated on the EVTO pin.
The EOS bits in DC must be set to 0xb10 to enable this feature. The EVTO pin can then be connected to
an external oscilloscope in order to examine watchpoint timing
Generating trace timing signals. Not used by the Atmel-ICE
8.2
debugWIRE Targets
8.2.1
Software Breakpoints
The debugWIRE OCD is drastically scaled down when compared to the Atmel megaAVR (JTAG) OCD. This
means that it does not have any program counter breakpoint comparators available to the user for debugging
purposes. One such comparator does exist for purposes of run-to-cursor and single-step operations, but user
breakpoints are not supported in hardware
Instead, the debugger must make use of the Atmel AVR BREAK instruction. This instruction can be placed
in FLASH, and when it is loaded for execution will cause the AVR CPU to enter stopped mode. To support
breakpoints during debugging, the debugger must insert a BREAK instruction into FLASH at the point at which
the users requests a breakpoint. The original instruction must be cached for later replacement. When single
stepping over a BREAK instruction, the debugger has to execute the original cached instruction in order to
preserve program behaviour. In extreme cases, the BREAK has to be removed from FLASH and replaced
later. All these scenarios can cause apparent delays when single stepping from breakpoints, which will be
exacerbated when the target clock frequency is very low.
It is thus recommended to observe the following guidelines, where possible:
Always run the target at as high a frequency as possible during debugging. The debugWIRE physical
interface is clocked from the target clock
Try to minimise on the number of breakpoint additions and removals, as each one require a FLASH page
to be replaced on the target
Try to add or remove a small number of breakpoints at a time, to minimise the number of FLASH page
write operations
If possible, avoid placing breakpoints on double-word instructions
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
32
9.
Special Considerations
9.1
Atmel AVR XMEGA OCD
OCD and clocking
When the MCU enters stopped mode, the OCD clock is used as MCU clock. The OCD clock is either the JTAG
TCK if the JTAG interface is being used, or the PDI_CLK if the PDI interface is being used.
I/O modules in stopped mode
In contrast to earlier Atmel megaAVR devices, in XMEGA the I/O modules are stopped in stop mode. This
means that USART transmissions will be interrupted, timers (and PWM) will be stopped.
Hardware breakpoints
There are four hardware breakpoint comparators - two address comparators and two value comparators. They
have certain restrictions:
All breakpoints must be of the same type (program or data)
All data breakpoints must be in the same memory area (IO, SRAM or XRAM)
There can only be one breakpoint if address range is used
Here are the different combinations that can be set:
Two single data or program address breakpoints
One data or program address range breakpoint
Two single data address breakpoints with single value compare
One data breakpoint with address range, value range or both
Atmel Studio will tell you if the breakpoint can't be set, and why. Data breakpoints have priority over program
breakpoints, if software breakpoints are available.
External reset and PDI physical
The PDI physical interface uses the reset line as clock. While debugging, the reset pullup should be 10k
or more or be removed. Any reset capacitors should be removed. Other external reset sources should be
disconnected.
Debugging with sleep for ATxmegaA1 rev H and earlier
There was a bug in the early versions of the ATxmegaA1 family that prevented the OCD to be enabled while
the device was in certain sleep modes. There are two methods to use to get back on the debugging:
Go into the Atmel-ICE Options in the Tools menu and enable "Always activate external reset when
reprogramming device"
Perform a chip erase
The sleep modes that trigger this bug are:
Power-down
Power-save
Standby
Extended standby
9.2
Atmel megaAVR OCD and debugWIRE OCD
IO Peripherals
Most I/O peripherals will continue to run even though the program execution is stopped by a breakpoint.
Example: If a breakpoint is reached during a UART transmission, the transmission will be completed and
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
33
corresponding bits set. The TXC (transmit complete) flag will be set and will be available on the next single step
of the code even though it normally would happen later in an actual device.
All I/O modules will continue to run in stopped mode with the following two exceptions:
Timer/Counters (configurable using the software front-end)
Watchdog Timer (always stopped to prevent resets during debugging)
Single Stepping I/O access
Since the I/O continues to run in stopped mode, care should be taken to avoid certain timing issues. For
example, the code:
OUT
PORTB, 0xAA<
IN
TEMP, PINB
When running this code normally, the TEMP register would not read back 0xAA because the data would not yet
have been latched physically to the pin by the time it is sampled by the IN operation. A NOP instruction must be
placed between the OUT and the IN instruction to ensure that the correct value is present in the PIN register.
However, when single stepping this function through the OCD, this code will always give 0xAA in the PIN
register since the I/O is running at full speed even when the core is stopped during the single stepping.
Single stepping and timing
Certain registers need to be read or written within a given number of cycles after enabling a control signal.
Since the I/O clock and peripherals continue to run at full speed in stopped mode, single stepping through such
code will not meet the timing requirements. Between two single steps, the I/O clock may have run millions of
cycles. To successfully read or write registers with such timing requirements, the whole read or write sequence
should be performed as an atomic operation running the device at full speed. This can be done by using a
macro or a function call to execute the code, or use the run-to-cursor function in the debugging environment.
Accessing 16-bit Registers
The Atmel AVR peripherals typically contain several 16-bit registers that can be accessed via the 8-bit data bus
(eg: TCNTn of a 16-bit timer). The 16-bit register must be byte accessed using two read or write operations.
Breaking in the middle of a 16-bit access or single stepping through this situation may result in erroneous
values.
Restricted I/O registeraccess
Certain registers cannot be read without affecting their contents. Such registers include those which contain
flags which are cleared by reading, or buffered data registers (eg: UDR). The software front-end will prevent
reading these registers when in stopped mode to preserve the intended non-intrusive nature of OCD
debugging. In addition, some registers cannot safely be written without side-effects occurring - these registers
are read-only. For example:
Flag registers, where a flag is cleared by writing '1' to any bit. These registers are read-only
UDR and SPDR registers cannot be read without affecting the state of the module. These registers are not
accessible
9.2.1
Atmel megaAVR OCD (JTAG)
Software breakpoints
Since it contains an early version of the OCD module, ATmega128[A] does not support the use of the BREAK
instruction for software breakpoints.
JTAG clock
The target clock frequency must be accurately specified in the software front-end before starting a debug
session. For synchronisation reasons, the JTAG TCK signal must be less than one fourth of the target clock
frequency for reliable debugging. When programming via the JTAG interface, the TCK frequency is limited by
the maximum frequency rating of the target device, and not the actual clock frequency being used.
When using the internal RC oscillator, be aware that the frequency may vary from device to device and is
affected by temperature and VCC changes. Be conservative when specifying the target clock frequency.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
34
See
"Debug Options" on page 28
for details on how to set the target clock frequency using the software front-
end.
JTAGEN and OCDEN fuses
The JTAG interface is enabled using the JTAGEN fuse, which is programmed by default. This allows access to
the JTAG programming interface. Through this mechanism, the OCDEN fuse can be programmed (by default
OCDEN is un-programmed). This allows access to the OCD in order to facilitate debugging the device. The
software front-end will always ensure that the OCDEN fuse is left un-programmed when terminating a session,
thereby restricting unnecessary power consumption by the OCD module. If the JTAGEN fuse is unintentionally
disabled, it can only be re-enabled using SPI or PP programming methods.
If the JTAGEN fuse is programmed, the JTAG interface can still be disabled in firmware by setting the JTD bit.
This will render code un-debuggable, and should not be done when attempting a debug session. If such code
is already executing on the Atmel AVR device when starting a debug session, the Atmel-ICE will assert the
RESET line while connecting. If this line is wired correctly, it will force the target AVR device into reset, thereby
allowing a JTAG connection.
If the JTAG interface is enabled, the JTAG pins cannot be used for alternative pin functions. They will remain
dedicated JTAG pins until either the JTAG interface is disabled by setting the JTD bit from the program code, or
by clearing the JTAGEN fuse through a programming interface.
Note
Be sure to check the "use external reset" checkbox in both the programming dialog and debug
options dialog in order to allow the Atmel-ICE to assert the RESET line and re-enable the JTAG
interface on devices which are running code which disables the JTAG interface by setting the JTD
bit.
IDR events
When the application program writes a byte of data to the OCDR register of the AVR device being debugged,
the Atmel-ICE reads this value out and displays it in the message window of the software front-end. The IDR
register is polled every 50ms, so writing to it at a higher frequency will NOT yield reliable results. When the
AVR device loses power while it is being debugged, spurious IDR events may be reported. This happens
because the Atmel-ICE may still poll the device as the target voltage drops below the AVR's minimum operating
voltage.
9.2.2
debugWIRE OCD
The debugWIRE communication pin (dW) is physically located on the same pin as the external reset (RESET).
An external reset source is therefore not supported when the debugWIRE interface is enabled.
The debugWIRE Enable fuse (DWEN) must be set on the target device in order for the debugWIRE interface
to function. This fuse is by default un-programmed when the Atmel AVR device is shipped from the factory. The
debugWIRE interface itself cannot be used to set this fuse. In order to set the DWEN fuse, SPI mode must be
used. The software front-end handles this automatically provided that the necessary SPI pins are connected. It
can also be set using SPI programming from the Atmel Studio programming dialog.
Either:
Attempt to start a debug session on the debugWIRE part. If the debugWIRE interface is not enabled, Atmel
Studio will offer to retry, or attempt to enable debugWIRE using SPI programming. If you have the full SPI
header connected, debugWIRE will be enabled, and you will be asked to toggle power on the target - this
is required for the fuse changes to be effective.
Or:
Open the programming dialog in SPI mode, and verify that the signature matches the correct device.
Check the DWEN fuse to enable debugWIRE.
Note
It is important to leave the SPIEN fuse programmed, the RSTDISBL fuse unprogrammed! Not
doing this will render the device stuck in debugWIRE mode, and high-voltage programming
will be required to revert the DWEN setting.
To disable the debugWIRE interface, use high-voltage programming to unprogram the DWEN fuse. Alternately,
use the debugWIRE interface itself to temporarily disable itself, which will allow SPI programming to take place,
provided that the SPIEN fuse is set.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
35
Note
If the SPIEN fuse was NOT left programmed, Atmel Studio will not be able to complete this
operation, and high-voltage programming must be used.
During a debug session, select the 'Disable debugWIRE and Close' menu option from the 'Debug' menu.
DebugWIRE will be temporarily disabled, and Atmel Studio will use SPI programming to unprogram the
DWEN fuse
Having the DWEN fuse programmed enables some parts of the clock system to be running in all sleep modes.
This will increase the power consumption of the AVR while in sleep modes. The DWEN Fuse should therefore
always be disabled when debugWIRE is not used.
When designing a target application PCB where debugWIRE will be used, the following considerations must be
made for correct operation:
Pull-up resistors on the dW/(RESET) line must not be smaller (stronger) than 10kΩ. The pull-up resistor is
not required for debugWIRE functionality, since the debugger tool provides this
Connecting the RESET pin directly to VCC will cause the debugWIRE interface to fail, and may result in
hardware damage to the Atmel-ICE
Any stabilising capacitor connected to the RESET pin must be disconnected when using debugWIRE,
since they will interfere with correct operation of the interface
All external reset sources or other active drivers on the RESET line must be disconnected, since they may
interfere with the correct operation of the interface
Never program the lock-bits on the target device. The debugWIRE interface requires that lock-bits are cleared
in order to function correctly.
9.3
Atmel AVR UC3 OCD
JTAG interface
On some Atmel AVR UC3 devices the JTAG port is not enabled by default. When using these devices it is
essential to connect the RESET line so that the Atmel-ICE can enable the JTAG interface.
aWire interface
The baud rate of aWire communications depends upon the frequency of the system clock, since data must
be synchronised between these two domains. The Atmel-ICE will automatically detect that the system clock
has been lowered, and re-calibrate its baud rate accordingly. The automatic calibration only works down to a
system clock frequency of 8kHz. Switching to a lower system clock during a debug session may cause contact
with the target to be lost.
If required, the aWire baud rate can be restricted by setting the aWire clock parameter. Automatic detection will
still work, but a ceiling value will be imposed on the results.
Any stabilising capacitor connected to the RESET pin must be disconnected when using aWire since it
will interfere with correct operation of the interface. A weak external pullup (10kΩ or higher) on this line is
recommended.
Shutdown sleep mode
Some AVR UC3 devices have an internal regulator that can be used in 3.3V supply mode with 1.8V regulated
I/O lines. This means that the internal regulator powers both the core and most of the I/O. The Atmel-ICE does
not support the Shutdown sleep mode were this regulator is shut off. In other words this sleep mode cannot be
used during debugging. If it is a requirement to use this sleep mode during debugging, use an Atmel AVR ONE!
debugger instead.
9.4
SAM / Coresight OCD
Some SAM devices include an ERASE pin which is asserted to perform a complete chip erase and unlock
devices on which the security bit is set. This pin is NOT routed to any debug header, and thus the Atmel-ICE is
unable to unlock a device. In such cases the user should perform the erase before starting a debug session.
JTAG interface
The RESET line should always be connected so that the Atmel-ICE can enable the JTAG interface.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
36
SWD interface
The RESET line should always be connected so that the Atmel-ICE can enable the SWD interface.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
37
10.
Firmware Upgrade
For information on how to upgrade the firmware, see the
Atmel Studio user guide
in
Atmel Studio (USER
GUIDE)
.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
38
11.
Release History and Known issues
11.1
What's New
Atmel-ICE is new!
11.2
Firmware Release History
11.2.1
Atmel Studio 6.2
Table 11-1. New in this Release
Release platform
Atmel Studio 6.2 (final)
Firmware version
1.13
New features
None
Fixes
Fixed oscillator calibration command
Improved debugWIRE reliability
11.2.2
Atmel Studio 6.2 (beta)2
Table 11-2. New in this Release
Release platform
Atmel Studio 6.2 (beta)
Firmware version
1.09
New features
First release of Atmel-ICE
Fixes
N/A
11.3
Known Issues Concerning the Atmel-ICE
11.3.1
Atmel AVR XMEGA OCD Specific Issues
For the ATxmegaA1 family, only revision G or later is supported
11.3.2
Atmel megaAVR OCD and Atmel tinyAVR OCD Specific Issues
Cycling power on ATmega32U6 during a debug session may cause a loss of contact with the device
11.4
Device Support
For a full device support table for all Atmel Tools, see the
"Supported Devices"
in
Atmel Studio (USER GUIDE)
.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
39
12.
Product Compliance
12.1
RoHS and WEEE
The Atmel-ICE (all kits) and its accessories are manufactured in accordance to both the RoHS Directive
(2002/95/EC) and the WEEE Directive (2002/96/EC).
12.2
CE and FCC
The Atmel-ICE unit has been tested in accordance to the essential requirements and other relevant provisions
of Directives:
Directive 2004/108/EC (class B)
FCC part 15 subpart B
2002/95/EC (RoHS, WEEE)
The following standards are used for evaluation:
EN 61000-6-1 (2007)
EN 61000-6-3 (2007) + A1(2011)
FCC CFR 47 Part 15 (2013)
The Technical Construction File is located at:
Atmel Norway
Vestre Rosten 79
7075 Tiller
Norway
Every effort has been made to minimise electromagnetic emissions from this product. However, under
certain conditions, the system (this product connected to a target application circuit) may emit individual
electromagnetic component frequencies which exceed the maximum values allowed by the abovementioned
standards. The frequency and magnitude of the emissions will be determined by several factors, including
layout and routing of the target application with which the product is used.
Atmel-ICE [USER GUIDE]
42330A-MCU-07/2014
40
13.
Document Revisions
Document
revision
Date
Comment
42330A
06/2014
Initial document for release.
Atmel Corporation
1600 Technology Drive, San Jose, CA 95110 USA
T:
(+1)(408) 441.0311
F:
(+1)(408) 436.4200
|
www.atmel.com
© 2014 Atmel Corporation. / Rev.: 42330A-MCU-07/2014
Atmel
®
, Atmel logo and combinations thereof, Enabling Unlimited Possibilities
®
, AVR
®
, AVR Studio
®
, megaAVR
®
, tinyAVR
®
, XMEGA
®
, and others are registered
trademarks or trademarks of Atmel Corporation in U.S. and other countries. ARM
®
, ARM Connected
®
, Cortex
®
logo and others are the registered trademarks or
trademarks of ARM Ltd. Windows
®
is a registered trademark of Microsoft Corporation in the U.S. and other countries. Other terms and product names may be
trademarks of others.
DISCLAIMER: The information in this document is provided in connection with Atmel products. No license, express or implied, by estoppel or otherwise, to any intellectual property right is granted
by this document or in connection with the sale of Atmel products. EXCEPT AS SET FORTH IN THE ATMEL TERMS AND CONDITIONS OF SALES LOCATED ON THE ATMEL WEBSITE,
ATMEL ASSUMES NO LIABILITY WHATSOEVER AND DISCLAIMS ANY EXPRESS, IMPLIED OR STATUTORY WARRANTY RELATING TO ITS PRODUCTS INCLUDING, BUT NOT LIMITED
TO, THE IMPLIED WARRANTY OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, OR NON-INFRINGEMENT. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT,
INDIRECT, CONSEQUENTIAL, PUNITIVE, SPECIAL OR INCIDENTAL DAMAGES (INCLUDING, WITHOUT LIMITATION, DAMAGES FOR LOSS AND PROFITS, BUSINESS INTERRUPTION,
OR LOSS OF INFORMATION) ARISING OUT OF THE USE OR INABILITY TO USE THIS DOCUMENT, EVEN IF ATMEL HAS BEEN ADVISED OF THE POSSIBILITY OF SUCH DAMAGES.
Atmel makes no representations or warranties with respect to the accuracy or completeness of the contents of this document and reserves the right to make changes to specifications and products
descriptions at any time without notice. Atmel does not make any commitment to update the information contained herein. Unless specifically provided otherwise, Atmel products are not suitable
for, and shall not be used in, automotive applications. Atmel products are not intended, authorized, or warranted for use as components in applications intended to support or sustain life.
SAFETY-CRITICAL, MILITARY, AND AUTOMOTIVE APPLICATIONS DISCLAIMER: Atmel products are not designed for and will not be used in connection with any applications where the failure
of such products would reasonably be expected to result in significant personal injury or death ("Safety-Critical Applications") without an Atmel officer's specific written consent. Safety-Critical
Applications include, without limitation, life support devices and systems, equipment or systems for the operation of nuclear facilities and weapons systems. Atmel products are not designed
nor intended for use in military or aerospace applications or environments unless specifically designated by Atmel as military- grade. Atmel products are not designed nor intended for use in
automotive applications unless specifically designated by Atmel as automotive-grade.