Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
PMIC: CP240x LCD Driver Family Slide 11
In order to reduce pin counts of displays and the controllers used to drive them a multiplex scheme is used. Unlike the static mode, a multiplexed display connects multiple segments together as shown in the figure. Here four segments are connected together which is called 4-mux mode. In addition, a multiplexed mode display also has multiple common references and the number of commons is equal to the mux mode. In the figure, there are 4 commons. Each of the four segments that are connected to a single pin such as 8A, 8B, 8C, and DP8, is referenced to one of the four commons. In the figure DP8 is referenced to COM0 whereas 8C is referenced to COM1.
PTM Published on: 2011-05-13