Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
PMIC: CP240x LCD Driver Family Slide 5
The fact that light is an electromagnetic wave that is visible to the eye is one basic principle that liquid crystal displays are based. Light sources emit the light waves in numerous directions or axis as represented by the series of arrows originating from the source shown above. Adding to that, each wave can be broken down to its orthogonal components meaning that each vector has a vertical and horizontal component to it. If a wave with a completely aligned vertical axis was examined its horizontal component would be zero. The reverse is also true regarding a wave aligned on the horizontal axis. Its vertical component is zero. Polarization relates to the orientation of the light waves and a polarizing filter allows only waves aligned on the specific axis to pass. The diagram above shows the result of two polarizing filters oriented 90 degrees out of phase. The first filter passes only the light waves that have a vertical orientation. The second filter will block the remaining light since that vertical waves have no horizontal component.
PTM Published on: 2011-05-13