Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
PMIC: CP240x LCD Driver Family Slide 35
Arbitration on the SMBus is possible due to the open drain configuration of the drivers. If the output is to be a logic 1 then the output of the drivers are tri-stated and the external pull-up resistor determines the logic level. If the output is to be a logic 0 then the output is driven to 0V. Therefore when the output is high, any driver on the bus can pull the output low. If two masters start transmitting at the same time and one drives a logic 0 while the other drives a logic 1, the device that drives the bus low will win arbitration.
PTM Published on: 2011-05-13